Water is truly the giver of life, and without it, life itself is simply not possible. Humans, plants, and animals—entire ecosystems and food chains—depend upon clean water to survive. But while nearly 70% of the world is covered by water, only 2.5% of it is fresh and fit for use and consumption. The remainder is saline and ocean-based. Beyond this, just 1% of our freshwater is easily accessible, with much of that trapped in glaciers and snow. And it seems the danger signs are growing as the UN reports by 2025, an estimated 1.8 billion people will live in areas plagued by water scarcity, with two-thirds of the world's population living in water-stressed regions as a result of use, growth, and climate change.
View the full article on the Analog.com website.